Du søgte efter:

AB-PM

Viser 322 produkt (er)

134B9696

iC7 Motion Drive-Train Model

The drive-train model contains the same assets as the drive model and an
additional motor model. Certain IM and PM motors can be selected from
the Motor menu to be modeled in the motor hardware plant part. A load
model must be connected externally, and external motor speed has to be
fed back to the drive-train model.

134B9699

iC7 Propulsion Drive-Train Model

The drive-train model contains the same assets as the drive model and an
additional motor model. Certain IM and PM motors can be selected from
the Motor menu to be modeled in the motor hardware plant part. A load
model must be connected externally, and external motor speed has to be
fed back to the drive-train model.

Vis: